AXIS#.VL.FBUNFILTERED

Description

AXIS#.VL.FBUNFILTERED reads the raw velocity feedback before any filters affect the value of this feedback.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read Only

Units

Depends on AXIS#.UNIT.VROTARY

Rotary: rpm, rps, deg/s, (custom units)/s, rad/s

Range

N/A

Default Value

N/A

Data Type

Float

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.VL.FBUNFILTERED

5011h

2bh

Signed32

-

1000:1

Read only

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6035

1

6035 (0x1793)

AXIS1.VL.FBUNFILTERED

Signed32

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.VL.FBUNFILTERED

6035

Float

Read Only

Velocity

Related Topics

Velocity Loop